Johnson Controls electrifies energy-intensive industries with new heat pumps that can triple energy efficiency and lower operating costs

Share

CORK, Ireland, Sept. 15, 2026 – Johnson Controls (NYSE: JCI), a global leader in thermal management, mission-critical building systems, energy efficiency, and decarbonization, today announced the launch of its Sabroe HitemHP line of industrial high-temperature heat pumps designed to help industries requiring high-temperature process heat in the Middle East to electrify and decarbonize, without compromising performance. In one specific customer application , the system delivered up to three times the energy efficiency of electric boilers while reducing energy costs by more than 91%, annual water costs by up to 30%, and on-site CO₂ emissions by up to 82% when paired with waste heat from a refrigeration plant.

A wave of growth across pharmaceuticals, biotechnology, advanced manufacturing, and food and beverage processing is driving demand for tighter, more energy-intensive operating conditions. At the same time, industrial heating remains a major challenge, particularly for processes requiring temperatures above 100°C, where businesses have traditionally relied on fossil fuel-based systems, difficult to decarbonize, and increasingly exposed to energy price volatility. The HitemHP range is built for this new reality. Engineered and manufactured in Europe, it enables customers to be resilient in the face of energy-related challenges by reducing energy costs and emissions, improving efficiency, and accelerating decarbonization while ensuring reliable operations and outcomes.

“The UAE Energy Strategy aims to reduce emissions from the water and energy sectors to ensure they achieve net zero by 2050,” said Devrim Tekeli, vice president and general manager, MEA, Johnson Controls. “With our new Sabroe high-temperature heat pumps, Johnson Controls is delivering a breakthrough solution that can help critical industries and institutions secure their energy future, significantly cut operational costs and align with regional industrial modernization, energy efficiency and decarbonization ambitions.”

Engineered and manufactured in Europe at the company’s advanced heat pump and chiller facility in Holme, Denmark, the HitemHP range uses only natural refrigerants. At the heart of the system is the proven Sabroe SMC single-stage reciprocating compressor, an aerodynamic innovation engineered for exceptional reliability, even under part-load conditions. This extends service intervals by nearly 50% while also improving energy performance.

Under part-load operation, the system can achieve up to 20% higher coefficient of performance (COP) than when operating at full capacity, helping reduce electricity consumption and operating costs.

Additional key features include:

  • Operational flexibility: Works across a wide range of heat sources, with capacity that can scale from 100% down to 18%, matching its output to the building’s needs to save energy and reduce wear.
  • Future-proof refrigerants: Uses ultra-low GWP butane and iso-butane.
  • Standardized, modular design: A configure-to-order approach reduces lead times, costs and installation complexity. Compact, factory assembled units enable fast commissioning.

The HitemHP market-leading features and exceptional range reflect input directly from customers who partnered with Jonhson Controls experts at the company’s state-of-the-art testing facility in Holme, Denmark.

Johnson Controls has been a heat pump pioneer for decades and today offers one of the industry’s most comprehensive portfolios of low- and ultra-low GWP solutions.

For more information visit Industrial Heat Pumps.



1Based on a customer application, using site-specific conditions including energy prices, and assumptions around water volumes and water quality requirements.

 

###


About Johnson Controls

Johnson Controls, a global leader in thermal management, mission-critical building systems, energy efficiency, and decarbonization, helps customers use energy more productively, reduce carbon emissions, and operate with the precision and resilience required in rapidly expanding industries such as data centers, healthcare, pharmaceuticals, advanced manufacturing, and higher education.

For more than 140 years, Johnson Controls has delivered performance where it really matters. Backed by advanced technology, lifecycle services and an industry-leading field organization, we elevate customer performance, turn goals into real-world results and help move society forward.

Visit johnsoncontrols.com for more information and follow @Johnsoncontrols on social platforms.

Share