Meet Metasys 16.0
Webinar and live Q&A | Tuesday, September 8, 2026 | 13:00 - 14:00 GST
 

Join this session to explore the release of Metasys 16.0. Discover how new capabilities in native redundancy, built-in cybersecurity and faster deployment help building owners, operators and engineers maximize uptime, reduce risk and streamline operations. Learn how enhanced energy insights, scalable architecture and accelerated engineering workflows can lower total cost of ownership while supporting compliance and decarbonization goals. See how Metasys 16.0 empowers teams to make better, data-driven decisions and optimize building performance.

By attending, you'll not only gain first-hand insight into the latest Metasys innovations, but you'll also be automatically entered into an exclusive attendee prize draw.

Metasys 16

What you'll discover:

  • Native server redundancy maintains continuous performance through multiple servers, that operate in tandem and keep facilities running 24/7
  • Built-in cybersecurity protects every layer of the BAS with encrypted communications, zero trust architecture and alignment with IEC 62443-4-2 Security Level 2
  • Fast track upgrade tool standardizes workflow and simplifies system management, reducing upgrade time by up to 40%
  • Flexibility for growth - scale easily from a single building to large campuses and portfolios, supporting up to 1.300 IP devices (30% more than previous versions)
  • EPBD-ready energy monitoring, including significant hours of engineering labor savings and enhanced data visualization.

Explore the release of Metasys 16.0 and uncover how it's empowering teams to make better, data-driven decisions and optimize building performance

Register today

Presented by:

Yehia Kamel

Yehia Kamel

Product Manager, EMEA Building Automation

Jemy Rajan

Jemy Rajan

Product Manager MEA Building Automation