- Johnson Controls
- Insights
- Cutting Costs and Reducing Loss With Visual Verification for Security Alarms
Cutting costs and reducing loss with visual verification for security alarms
Alarm verification is an important step to enhance security systems. Such a system will help regulate the response to false alarms due to user error-a particular help to the police-while not compromising on the security needs of people.
Visual Verification Systems use Passive Infrared or PIR motion cameras to capture the incident and send video clips to the monitoring station for further investigation. This white paper explains the features of the visual verification systems and the reasons to opt for it.
























.jpg?la=en-ZW&h=320&w=720&hash=A40D709EBC2BC33ED5B5438DAE8A3F42)














.jpg?la=en-ZW&h=310&w=720&hash=57A5D8DBDBB70BA989FE342E97FC7B8C)


.jpg?la=en-ZW&h=320&w=719&hash=60BB26AE1EE6030C04BB4E0C1E94B0EC)
.jpg?la=en-ZW&h=306&w=720&hash=85191C5ECD82203B545F5B73E28C65C5)

.png?la=en-ZW&h=320&w=720&hash=7338885F69DE18696FE749CBAEF250C7)