- Johnson Controls
- Insights
- Wings Case Study
Groundbreaking property succeeds with groundbreaking BAS
When a new hospitality initiative in Belgium had its sights on comfort, sustainability and occupant well-being, little did they know they’d become Europe’s first-ever triple-certified building—while realizing energy savings. Read the story of The Wings.
Developing an exciting hospitality complex called The Wings in Belgium also meant prioritizing comfort, well-being and sustainability for the facility. Using its Metasys building automation system, Johnson Controls helped create a building concept that provided the perfect balance of business and leisure—in a modern and sustainably advanced environment. This allowed The Wings to optimize building performance, mitigate risk and have sustainable operations.
When it was complete, The Wings became Europe’s first-ever building to be triple certified, earning BREEAM Excellent, WELL Gold, and DGNB Gold designations.
Read about this exciting journey, and the challenges along the way, in our latest case study: Read the case study
























.jpg?la=en-ZW&h=320&w=720&hash=A40D709EBC2BC33ED5B5438DAE8A3F42)














.jpg?la=en-ZW&h=310&w=720&hash=57A5D8DBDBB70BA989FE342E97FC7B8C)


.jpg?la=en-ZW&h=320&w=719&hash=60BB26AE1EE6030C04BB4E0C1E94B0EC)
.jpg?la=en-ZW&h=306&w=720&hash=85191C5ECD82203B545F5B73E28C65C5)

.png?la=en-ZW&h=320&w=720&hash=7338885F69DE18696FE749CBAEF250C7)