- Johnson Controls
- Industrial Refrigeration and Heating
- Commercial Heat Pump Solutions
Heat Pumps
Hit decarbonisation targets whilst providing efficient, cost-effective environmental controlCutting energy costs with sustainable Heating Solutions
As the drive towards decarbonisation and environmentally friendly solutions to heating and cooling accelerate, Johnson Controls is at the forefront of the technological revolution to design, manufacture, install, and service ultra-energy efficient HVAC products such as water and air source heating pumps.
Our range of easy-to-install water and air source heating pumps deliver a renewable solution to heating and cooling applications that reduce energy bills and provide you with a low carbon footprint solution.
Integrating air source or water source heating into your HVAC system is a great solution for most commercial buildings, as the installation is quick and easy, and you don’t need much space to mount your air source heating unit outside.
Get the full breakdown of how air source heating systems work and how they can reduce your heating overheads in our latest article.
Combining this renewable energy source with our proven environment controls, Johnson Controls can maintain your building at an optimum temperature whilst satisfying your net zero commitments.
How does a Heat Pump work?
A heat pump extracts heat from the outside air, or local water sources, even at low temperatures, and converts it into energy that you can use within your building's heating or cooling system.
This low-cost, low-impact energy can maintain indoor temperatures at ideal conditions, provide hot water, and help your business meet its decarbonisation goals.
High capacity reciprocating Heat Pumps
High capacity screw Heat Pump
HyePac high temperature heat pump
Different types of Heat Pump
Johnson Controls offer a range of heat pump solutions, each designed to suit specific applications. The different types of heat pumps available include:
Commercial air source Heat Pumps
Commercial air source heat pumps (ASHPs) efficiently heat and cool large buildings by extracting heat from the outdoor air using an evaporator coil. The heat is then amplified through compression before being released indoors, creating a comfortable environment. ASHPs are a cost-effective and eco-friendly solution for commercial heating and cooling needs.

Commercial water source Heat Pumps
Our water source heat pumps work by extracting heat from local water sources such as lakes or wells, even at low temperatures. This heat is and converted into energy that can be used within your building’s heating or cooling system. This low-cost, low-impact energy can maintain indoor temperatures, provide hot water, and help you meet decarbonisation goals.

Water source heat pumps are only a viable source of energy if your business premises are near a useable water source, so while they’re an excellent choice, they won’t be suitable for all applications.
Please note that we do not currently install heat pumps for small domestic buildings.
Reclaiming waste hot air from chillers
Waste heat is often released into the atmosphere by chilling air for internal building cooling.
Air source heat pumps harness heat recovery technologies to convert waste hot air into an energy source. Our solutions can effectively recycle it to power other elements of your HVAC system, such as hot water. This can significantly increase your air source heating system efficiency and reduce energy consumption.
What are the key benefits of using a Heat Pump from Johnson Controls?
Switching to an air source heating system
Find out how these energy savings translate into business savings in our latest article.
Learn more
Johnson Controls as a service – the future of sustainable building performance
Achieve goals, make strategic financial choices, and oversee the setup, maintenance, and connectivity of your building's infrastructure - all at a predictable monthly cost. We provide uninterrupted assistance, month after month, enabling you to concentrate on your primary operations while enjoying the lasting advantages of collaborating with Johnson Controls.
Learn moreComprehensive HVAC-R solutions
Johnson Controls offer a complete range of heating, ventilation, air-conditioning and refrigeration (HVAC-R) solutions. No matter what size of facility you manage, we can meet your requirements and surpass them.
Our solutions include a wide range of award-winning products from recognised brands, including York and Metasys.
We can provide industry-leading products, including ground, water and air source heating pumps, chillers, air handling units, fan coil units, air distribution products, close control air conditioning units, and management systems.
























.jpg?la=en-ZW&h=320&w=720&hash=A40D709EBC2BC33ED5B5438DAE8A3F42)














.jpg?la=en-ZW&h=310&w=720&hash=57A5D8DBDBB70BA989FE342E97FC7B8C)


.jpg?la=en-ZW&h=320&w=719&hash=60BB26AE1EE6030C04BB4E0C1E94B0EC)
.jpg?la=en-ZW&h=306&w=720&hash=85191C5ECD82203B545F5B73E28C65C5)

.png?la=en-ZW&h=320&w=720&hash=7338885F69DE18696FE749CBAEF250C7)