Cutting Energy Costs With Sustainable Heating Solutions

As the drive towards decarbonisation and environmentally friendly solutions to heating and cooling accelerate, Johnson Controls is at the forefront of the technological revolution to design, manufacture, install, and service ultra-energy efficient HVAC products such as water and air source heating pumps.

Our range of easy-to-install water and air source heating pumps deliver a renewable solution to heating and cooling applications that reduce energy bills and provide you with a low carbon footprint solution.

Integrating air source or water source heating into your HVAC system is a great solution for most commercial buildings, as the installation is quick and easy, and you don’t need much space to mount your air source heating unit outside.

Get the full breakdown of how air source heating systems work and how they can reduce your heating overheads in our latest article.

Combining this renewable energy source with our proven environment controls, Johnson Controls can maintain your building at an optimum temperature whilst satisfying your net zero commitments.

two york air cooled chillers jci

How does a Heat Pump work?

A heat pump extracts heat from the outside air, or local water sources, even at low temperatures, and converts it into energy that you can use within your building's heating or cooling system.

This low-cost, low-impact energy can maintain indoor temperatures at ideal conditions, provide hot water, and help your business meet its decarbonisation goals.

Different Types of Heat Pump

Johnson Controls offer a range of heat pump solutions, each designed to suit specific applications. The different types of heat pumps available include:

An industrial heat pump on a white background

Commercial and Industrial Spaces - Warming up to Heat Pumps

There is growing global demand for a 360° net zero carbon solution. Businesses, government and global coalitions have all set ambitious sustainability goals over the next two decades, with many aspiring for decarbonisation by 2030. These have spurred the switch to heat pumps in commercial buildings, factories and public facilities across the globe, and increasingly, within Singapore. Heat pumps could satisfy 80% of global heating and cooling needs with a lower carbon footprint than boilers using fossil fuels.
Read Full Article
Illustration of hvac air source heat pumps

Air Source Heat Pumps

Commercial air source heat pumps (ASHPs) efficiently heat and cool large buildings by extracting heat from the outdoor air using an evaporator coil. The heat is then amplified through compression before being released indoors, creating a comfortable environment. ASHPs are a cost-effective and eco-friendly solution for commercial heating and cooling needs.

Illustration of hvac water source heat pumps

Water Source Heat Pumps

Our water source heat pumps work by extracting heat from local water sources such as lakes or wells, even at low temperatures. This heat is and converted into energy that can be used within your building’s heating or cooling system. This low-cost, low-impact energy can maintain indoor temperatures, provide hot water, and help you meet decarbonisation goals.

Products

Sabroe Heat Pumps

York Heat Pumps

Frick Heat Pumps

Reclaiming Waste Hot Air from Chillers

Waste heat is often released into the atmosphere by chilling air for internal building cooling.

Air source heat pumps harness heat recovery technologies to convert waste hot air into an energy source. Our solutions can effectively recycle it to power other elements of your HVAC system, such as hot water. This can significantly increase your air source heating system efficiency and reduce energy consumption. 

Contact us to learn more
Frog's eye view of tall buildings

What are the key benefits of using a Heat Pump from Johnson Controls?

Low Energy Usage
Up to 70% of the energy used by an air source heating pump is extracted from the outside air, significantly reducing the need for increasingly expensive electricity.
Efficient Heating
When compared to traditional gas boilers powered by fossil fuel, Heat Pumps can be up to 500% more efficient, which can radically reduce energy costs.
Reduced Carbon Footprint
As most of the energy used to generate heat through a Heat Pump is renewable, installing Heat Pumps can significantly contribute to your organisation’s decarbonisation targets.
Friendly to the Local Environment
Because Heat Pumps do not burn oil, gas, LPG or biomass, or generate fumes of any kind, the air quality in the local area will not be affected in any way. This clean, renewable energy source can be vital when installed in buildings such as schools.
Proven Technologies
Johnson Controls is at the cutting edge of Heat Pump technology. Our solutions have been successfully installed worldwide, providing our customers with cheaper, cleaner HVAC solutions.
Low Cost Service and Maintenance
The Heat Pump solutions supplied from Johnson Controls allow easy access to the system components in order to make maintenance easier and reduce down times and servicing costs.
Easy to Install
Our Heat Pumps can be installed quickly and easily, meaning you can enjoy the cost benefits immediately.
Manufactured in Europe
Our Heat Pump solutions are manufactured in our European facilities, protecting our supply chain and allowing faster delivery times.
HVAC Experience
Johnson Controls has been an innovator within the HVAC industry for over 130 years and has a wide breadth of experience in designing, installing, commissioning and maintaining state-of-the-art heating, cooling, and air conditioning systems.

Product Portfolio

We offer a complete range of products with wide range of commercial applications (from 100 sqm to million sqm) from Sabroe and York that are customized to suit your goals and requirements. We will work with you to find the optimum solution and seek the subject matter experts in our organization to provide optimum support for each project.

Johnson Controls holds a large portfolio which span across refrigerants, technologies and compressor types, thereby enabling us to optimize a solution for each individual customer which will maximize the project investment. We support projects from the cradle/discovery/feasibility to commissioning and throughout the value generation with after-market solutions

Our industrial products are manufactured in our own factories thereby protecting supply chains and allowing full visibility through the project process.
Top view of three lakes forming the recycling symbol amidst a lush forest

Switching To An Air Source Heating System

Find out how these energy savings translate into business savings in our latest article.

Learn more

Check out our other Industrial Refrigeration and HVAC Products here:

Our Brands

YORK logo
Sabroe logo
Frick Industrial Refrigeration logo

Stay one step ahead with news and insights from our HVAC equipment experts.

Oil and petrochemical factory at night

De-Carbonized Cooling and Heating with Absorption Technology

Absorption chillers / heat pumps transfer energy from waste heat source to deliver de-carbonized cooling and heating for commercial, industrial, district energy and even marine applications.

Frick High Pressure Screw heat pump

Heat Pumps in ASEAN: The Key to Meeting Net Zero Targets?

In the drive towards reduction of CO2 emission to achieve a net zero goal in ASEAN and across Asia, heat pumps are integral to ensuring a sustainable future

Cityscape across a lush park during a cloudy day

Heat Pump or Boiler: What is the Business Case?

Managing energy consumption for the heating and cooling of buildings and industry is essential if nations are to achieve global carbon reduction and sustainability goals.

Two construction workers in protective glasses, clothing and helmet

Johnson Controls As a Service

Achieve goals, make strategic financial choices, and oversee the setup, maintenance, and connectivity of your building's infrastructure - all at a predictable monthly cost.

Heat Pump equipment

Beijing Municipal Administrative Center

Eco-project sets the standards for smart, clean urban living using renewable energy-powered heat pumps

Contact us to discuss your Heat Pump requirements with one of our experts

 

This form collects your name, email address and other personal information. Please read our Privacy Notice for information on how we protect and manage your personal data. By completing this form and submitting your information, you confirm that you agree to be contacted by Johnson Controls and that you have reviewed, understood and accepted our privacy terms as well as our cookie terms.

Our full Terms of Use can be read by clicking here.

Please note that once you have subscribed to our email lists, you can unsubscribe, or change your email preferences at any time.